|
(Read-Write) Set and query the marker tracking state for the specified readout line. Select the parameter to track on the standard Marker Search menu. When set to ON, Peak tracking is set by default. To set a different marker search function, use the standard Calc:Mark:Function commands. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<x> |
Large Marker Display State to edit. Choose from: A or B Note: This is a SCPI node and not an argument. See example below. |
|
<n> |
Readout line number. Choose from 1, 2, or 3. |
|
<bool> |
Marker tracking state. Choose from: OFF or 0 - Tracking disabled. ON or 1 - Tracking enabled. |
|
Examples |
DISP:MARK:LARG:A:DEF:LINE1:TRACking 1 |
|
Query Syntax |
DISPlay:MARKer:LARGe:<x>:DEFine:LINE<n>:TRACking? |
|
Return Type |
Boolean |
|
Default |
OFF |
Last Modified:
|
22-Sept-2014 |
New command |