|
(Read-Write) Set and query the marker bandwidth search state for the specified trace. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<x> |
Large Marker Display State to edit. Choose from: A or B Note: This is a SCPI node and not an argument. See example below. |
|
<n> |
Trace number. Choose from 1, 2, or 3. |
|
<value> |
Marker bandwidth search state. Choose from: OFF or 0 - BW search is OFF. ON or 1 - BW search is ON. |
|
Examples |
DISP:MARK:LARG:A:DEF:TRAC1:BWID:STAT ON |
|
Query Syntax |
DISPlay:MARKer:LARGe:<x>:DEFine:TRACe<n>:BWIDth:STATe? |
|
Return Type |
Boolean |
|
Default |
OFF |
Last Modified:
|
22-Sept-2014 |
New command |