|
(Read-Write) Set and query the display format for the specified trace. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<x> |
Large Marker Display State to edit. Choose from: A or B Note: This is a SCPI node and not an argument. See example below. |
|
<n> |
Trace number. Choose from 1, 2, or 3. |
|
<value> |
Display format. Choose from: MLOGarithmic – Log magnitude MLINear – Linear magnitude SWR – Standing Wave Ratio PHASe - Phase in degrees. The trace wraps every 360 degrees, from +180 to –180 UPHase - Unwrapped phase in degrees. SMITh – Smith chart; series resistance and reactance. POLar - Magnitude and phase of the reflection coefficient. GDELay – Group delay
|
|
Examples |
DISP:MARK:LARG:A:DEF:TRAC1:FORM MLIN |
|
Query Syntax |
DISPlay:MARKer:LARGe:<x>:DEFine:TRACe<n>:FORMat? |
|
Return Type |
Character |
|
Default |
MLOG |
Last Modified:
|
22-Sept-2014 |
New command |