|
(Read-Write) Set and query the measurement to display for the specified trace. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<x> |
Large Marker Display State to edit. Choose from: A or B Note: This is a SCPI node and not an argument. See example below. |
|
<n> |
Trace number. Choose from 1, 2, or 3. |
|
<value> |
Measurement. Choose from:
|
|
Examples |
DISP:MARK:LARG:A:DEF:TRAC1:MEAS S11 |
|
Query Syntax |
DISPlay:MARKer:LARGe:<x>:DEFine:TRACe<n>:MEASurement? |
|
Return Type |
Character |
|
Default |
Trace1=S11 Trace2=S21 Trace1=S12 |
Last Modified:
|
22-Sept-2014 |
New command |