DISPlay:NREVm:WINDow<n>:CCARrier <string>

(Read-Write) Set and query the displayed component carrier (CC).

Relevant Modes

NR5G

Parameters

 

<n>

Window number. If unspecified, value is set to 1.

n = 1 | 2 | 3 | 4  (Up to four windows can be selected/active at one time on the FieldFox.)

<string>

Choices:

ALL: All component carriers are displayed that meet the current setup's measurement criteria

CC0:CC4: Component carrier 0: component carrier 4

Examples

DISP:NREVm:WIND2:CCAR ALL

DISP:NREVm:WIND4:CCAR CC4

Query Syntax

DISP:NREVm:WIND3:CCAR?

Return Type

string

Default

ALL


Last Modified:

11dec2019

New command