DISPlay:WINDow:TRACe:Y:DLINe:STATe <bool>

(Read-Write) Set and query the ON/OFF state of the Display Line. Use DISPlay:WINDow:TRACe:Y:DLINe to set the display level.

Relevant Modes

EMI, IQA, NF, SA, RTSA

Parameters

 

<boolean>

Choose from:

0 or OFF - Display Line OFF.

1 or ON - Display Line ON.

Examples

DISPlay:WINDow:TRAC:Y:DLIN:STAT 1

Query Syntax

DISPlay:WINDow:TRACe:Y:DLINe:STATe?

Return Type

boolean

Default

0 - OFF


Last Modified:

04no2022

Added EMI mode (12.3x)

01june2018

Added NF mode Opt. 356 (10.3)

22oct2017

Added IQA mode (10.1x)

10-june-2016

Added RTSA mode (9.50)

1-Aug-2011

New command