(Read-Write) Set and query the bottom (lower) Y-axis scale value. |
|
Relevant Modes |
CAT mode: this command always acts on the selected trace. Select a trace using CALCulate:PARameter:SELect SA - Read ONLY |
Parameters |
|
<n> |
NF and NA modes Only: Specify the displayed trace number. NA Only: Choose from 1 to 4. NF Only: Choose from 1 to 2. If unspecified, value is set to 1. |
<num> |
Bottom scale value. Units depend on the selected format. |
Examples |
DISP:WIND:TRAC1:Y:BOTT -50 |
Query Syntax |
DISPlay:WINDow:TRAC<n>:Y[:SCALe]:BOTTom? |
Return Type |
Numeric |
Default |
Depends on Mode |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
01june2018 |
Added NF mode Opt. 356 (10.3) |
23-Jan-2013 |
Modified again for CAT |
26-Apr-2012 |
Modified for CAT (5.75) |