This example shows how to:
Create a simple NA Mode setup with 4-window configuration
Set format, scale, frequency, IFBW, Averaging
Set triggering to Single
Read Data
Clear Averaging
|
Note: In the following example: "-p" indicates a user prompt. "#" indicates a comment This example can be copied into a text editor, saved as a *.txt file, and run using the free Keysight Instrument Console program. Learn more. |
|
# Preset Instrument and Hold *RST # Change to NA Mode and wait until changed INST:SEL "NA";*OPC? # 4 window configuration DISP:WIND:SPL D12_34 #change window 4 to R1 measurement CALC:PAR4:DEF R1 #Select window 4 CALC:PAR4:SEL #change window 4 format to SWR CALC:FORMat SWR # Autoscale window 1 DISP:WIND:TRAC1:Y:AUTO # Set Center Freq SENS:FREQ:CENT 2e9 # Set Freq Span SENS:FREQ:SPAN 500e6 #set IFBW to 10 kHz BWID 10e3 # Set averaging to 5 sweeps AVER:COUNt 5 #Select window 1 CALC:PAR1:SEL # Set to HOLD mode; wait INIT:CONT 0;*OPC? # Trigger FIVE measurements # Wait between each INIT:IMMediate;*OPC? INIT:IMMediate;*OPC? INIT:IMMediate;*OPC? INIT:IMMediate;*OPC? INIT:IMMediate;*OPC? #Read formatted data from selected trace (1) CALC:DATA:FDATa? #Clear averaging AVER:CLEar #And do anther sweep INIT:IMMediate;*OPC? |
Last Modified:
|
23-Aug-2011 |
New command |