The following example program illustrates how to parse block data using C#.
|
/// <summary> /// Generates a IEEE block header for the specified size. /// </summary> /// <remarks> /// The block header is of the form #[digit indicating number of digits to follow][length] /// e.g. 201 bytes -> "#3201 /// 9999 bytes -> "#49999" /// 0 bytes -> "#10" /// </remarks> /// <param name="size">Size of the block.</param> /// <returns>Block header size string.</returns> string GenerateBlockHeader(int size) { string sz = size.ToString(); return "#" + sz.Length.ToString() + sz; } /// <summary> /// Parses a partially digested IEEE block length header, and returns /// the specified byte length. /// </summary> /// <remarks> /// The Stream pointer is assumed to point to the 2nd character of the block header /// (the first digit of the actual length). The caller is assumed to have parsed the /// first two block header characters (#?, where ? is the number of digits to follow), /// and converted the "number of digits to follow" into the int argument to this function. /// </remarks> /// <param name="numDigits">Number of digits to read from the stream that make up the /// length in bytes.</param> /// <returns>The length of the block.</returns> int ReadLengthHeader(int numDigits) { string bytes = string.Empty; for (int i = 0; i < numDigits; ++i) bytes = bytes + (char)Stream.ReadByte(); return Convert.ToInt32(bytes); } |