INSTrument[:SELect] <string>

(Read-Write) Set and query the current operating mode. Use INST:CAT? to read the available modes on the FieldFox.

This command is overlapped. This means that it will execute and, while the FieldFox changes mode, it will also accept new commands. Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands.

Relevant Modes

ALL

Parameters

 

<string>

Operating Mode. Case-sensitive. Choose from the modes that are installed on your FieldFox:

  • "CAT"

  • "Channel Scanner"

  • "CPM"

  • "EMI"

  • "ERTA"

  • "IQ"

  • "NA"

  • "NF"

  • "OTA"

  • "Phased Array Antenna"

  • "Power Meter"

  • "Pulse Measurements"

  • "RS"

  • "RSTA"

  • "SA"

  • "VVM"

Examples

INST "NA";*OPC?

Query Syntax

INSTrument[:SELect]?

Default

Depends on FieldFox model


Last Modified:

05Oct2017

Added IQA mode (10.1x)