MMEMory:IMPort:PAMPlifier  <string>,<char>

(Write-only) Load a match data (*.csv or *.snp) file from the specified device.

  • Imports *.csv and *.snp files from the "NoiseFigure\Preamp" folder.

Note: Before importing a file, the file must be stored in the NoiseFigure\Preamp folder.

See also, MMEMory:LOAD:PAMPlifier and MMEMory:STORe:PAMPlifier.

See ALL MMEM commands.

Relevant Modes

NF

Parameters

 

<string>

*.csv or *.snp

<char>

Memory device where the match data file is stored. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:IMP:PAMP "MySNP.s2p",INT

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)