MMEMory:STORe:PAMPlifier  <string>,<char>

(Write-Only) Store an uncertainty preamplifier (*.amp) file to the specified device.

  • Preamplifier files (*.amp) are saved and recalled from the "NoiseFigure\AMP" folder. If the folder does not already exist on a USB or SD card, it is created automatically before storing the file.

Note: Template *.amp files for several common models of preamplifiers may be found in the default AMP table directory of the FieldFox. In these files, the reflection coefficients have been set to the values specified for the respective model numbers, but the values for the AMP or AMP uncertainty will need to be entered at each frequency.

See also, MMEMory:LOAD:PAMPlifier and MMEMory:IMPort:PAMPlifier.

See ALL MMEM commands.

Relevant Modes

NF

Parameters

 

<string>

For *.amp files, provide filename of the *.amp file WITHOUT an extension.

<char>

Memory device where the preamplifier file is stored. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:STOR:PAMP "MyAMP",INT

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)