:MMEMory:LOAD:LIST

(Write-only) Load a *.csv custom file.

See ALL MMEM commands.

Relevant Modes

ChScn

Parameters

 

<string>

For *.csv files, provide filename of the antenna file WITHOUT an extension.

<char>

Memory device where the Antenna file is stored. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:LOAD:ANT "ChanScan",INT

mmemory:load:antenna "demo_channel_3g.csv",internal

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified: