(Write-only) Load a match data (*.csv or *.snp) file from the specified device.
Note: Before importing a file, the file must be stored in the NoiseFigure\DUT folder. See also, MMEMory:STORe:DUT and MMEMory:LOAD:DUT. |
|
Relevant Modes |
|
Parameters |
|
<string> |
*.csv or *.snp |
<char> |
Memory device where the match data file is stored. Choose from the following:
|
Examples |
MMEM:IMP:DUT "MySNP.s2p",INT |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |