MMEMory:STORe:DUT  <string>,<char>

(Write-Only) Store a uncertainty DUT (*.dut) file to the specified device.

  • ENR files are saved and recalled from the "NoiseFigure\DUT" folder. If the folder does not already exist on a USB or SD card, it is created automatically before storing the file.

See also, MMEMory:LOAD:DUT and MMEMory:IMPort:DUT.

See ALL MMEM commands.

Relevant Modes

NF

Parameters

 

<string>

For *.dut files, provide filename of the *.dut file WITHOUT an extension.

<char>

Memory device where the DUT file is stored. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:STOR:DUT "MyDUT",INT

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)