|
Note: This command is replaced by RECPlayback:CONFig:FMTRigger:LLData which can be used with Relative masks. (Read-Write) Set and query the data to complete the Frequency Mask Trigger (FMT) table, used for Record Playback. Measured power levels above an upper limit and below a lower limit will trigger recording. For ACP measurements, use CALC:ACP:OFFS:LIST:LIMit:NEG[:UPPer]:DATA and CALC:ACP:OFFS:LIST:LIM:POS[:UPPer]:DATA. |
|||||||||||||
|
Relevant Modes |
SA |
||||||||||||
|
Parameters |
|
||||||||||||
|
<data> |
Data for all FMT segments in the following format:
Subsequent segments are appended to the data in the same manner. |
||||||||||||
|
Examples |
'The following writes three upper limit segments. ' individual segments are colored for readability. RECP:CONF:FMTR:DATA 3,1,0,2e7,3e7,-30,0,1,0,3e7,5e7,0,0,1,0,5e7,6e7,0,-30 |
||||||||||||
|
Query Syntax |
RECPlayback:CONFig:FMTRigger:DATA? |
||||||||||||
|
Return Type |
Block data |
||||||||||||
|
Default |
0 - Limit line data off |
||||||||||||
Last Modified:
|
16-Aug-2012 |
Superseded A.06.00 |