Note: This command replaces RECPlayback:CONFig:FMTRigger:DATA which can be used ONLY with a Fixed mask. This command can also be used with Relative masks. (Read-Write) Set and query the data to complete the Frequency Mask Trigger (FMT) table, used for Record Playback. Measured power levels above an upper limit and below a lower limit will trigger recording. For ACP measurements, use CALC:ACP:OFFS:LIST:LIMit:NEG[:UPPer]:DATA and CALC:ACP:OFFS:LIST:LIM:POS[:UPPer]:DATA. |
|||||||||||||||
Relevant Modes |
SA |
||||||||||||||
Parameters |
|
||||||||||||||
<data> |
Data for all FMT segments in the following format:
Subsequent points are appended to the data in the same manner. |
||||||||||||||
Examples |
'The following writes three upper segments. ' individual segments are colored for readability. RECP:CONF:FMTR:LLData 1,1,0,0,4,-30e6,-20,-20e6,-10,-10e6,0,10e6,0,20e6,-10,30e6,-20 |
||||||||||||||
Query Syntax |
RECPlayback:CONFig:FMTRigger:LLData? |
||||||||||||||
Return Type |
Block data |
||||||||||||||
Default |
0 - Limit line data off |
||||||||||||||
Last Modified:
16-Aug-2012 |
New command |