(Read-Write) Sets the first trace in the range of traces to be either played back or specified for CSV output from the currently-open Record/Playback session. (Opt 236). Note: For related information on using FTP to transfer files from the FieldFox to a PC, refer to and the FAQ for "Using FTP with FieldFox". See also, :RECP:CONF:PRLT and :RECP:SESS:CSST. |
|
Relevant Modes |
SA, RTSA |
Parameters |
n/a |
<integer> |
Sets the first trace in the displayed traces to be recorded to a CSV file. |
Examples |
RECP:CONF:PRFT 10 */Sets trace 10 as the first trace to be either played back or specified for CSV output in a range of trace data |
Query Syntax |
RECP:CONF:PRFT? |
Default |
0 |
Last Modified:
22-044-2026 |
New command A.11.25 |