(Read-Write) Sets the state of the standard CSV file Save operation to enable multiple traces to be moved from a Recording to a CSV file. (Opt 236 and Opt 350). Note: For related information on using FTP to transfer files from the FieldFox to a PC, refer to and the FAQ for "Using FTP with FieldFox". See also, :RECP:CONF:PRFT and :RECP:CONF:PLFT. |
|
Relevant Modes |
SA, RTSA |
Parameters |
SING (Default) - Save data from a single trace (the current on screen trace) to a CSV file. RANG - Save a range of trace data (x to y) from the current open RecordPlayback session to a CSV file. ALL - Save all of the traces from the current open RecordPlayback session to a CSV file. |
<string> |
Range type for the data being stored to a CSV file. |
Examples |
RECP:SESS:CSST ALL */Records all of the displayed trace(s) data to a CSV file. RECP:SESS:CSST RANG */Records the specified range of trace data RECP:SESS:CSST SING */Records only the current displayed trace's data |
Query Syntax |
RECP:SESS:CSST? |
Default |
SING |
Last Modified:
22-044-2026 |
New command |