(Write-Read) Set and query the de-emphasis τ (RC time constant). Note: The cutoff frequency is related to the RC time constant by the following equation:
See also ADEM:METR:FILT:DEEM. |
|
Relevant Modes |
|
Parameters |
|
<bool> |
Choose from: Min: 1 µs Max: 1 s |
Couplings |
None |
Examples |
ADEM:METR:FILT:DEEM:TAO .000005 'sets the de-emphasis RC time constant (TAO) to 5 µs. ADEM:METR:FILT:DEEM:TAO 5e-6 'sets the de-emphasis RC time constant (TAO) to 5 µs. |
Query Syntax |
ADEM:METR:FILT:DEEM:TAO? |
Default |
2.500000000E-05 |
Last Modified:
15june2021 |
New command (A.12.3x) |