|
(Read-Write) Set and query the custom HPF 3 dB cutoff frequency (this setting is only relevant when the Highpass Filter is set to Custom). See also ADEM:METR:FILT:HPF. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<num> |
The 3 dB cutoff frequency in Hz. Choose a value between 20 Hz and 5 MHz. Min: 20 Hz Max: 5 MHz |
|
Examples |
ADEM:METR:FILT:HPF:CUT 22KHZ 'Sets the 3 dB cutoff frequency to 22 kHz (Only valid, when the HPF is set CUSTom). ADEM:METR:FILT:HPF:CUT 1 MHz 'Sets the 3 dB cutoff frequency to 1 MHz (Only valid, when the HPF is set CUSTom). |
|
Query Syntax |
ADEM:METR:FILT:HPF:CUT? |
|
Return Type |
character |
|
Default |
500 Hz |
Last Modified:
|
14june2021 |
New command (A.12.3x) |