|
(Read-Write) Set and query the analog demod lowpass filter type (this setting is only relevant when the Lowpass Filter is set to Custom). See also ADEM:METR:FILT:LPF. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<char> |
Chose a lowpass filter type Choose a value between 90 Hz and 5 MHz Min: 90 Hz Max: 5 MHz |
|
Examples |
ADEM:METR:FILT:LPF:CUT 22KHZ 'Sets the 3 dB cutoff frequency to 22 kHz (Only valid, when the LPF is set CUSTom). ADEM:METR:FILT:LPF:CUT 1 MHz 'Sets the 3 dB cutoff frequency to 1 MHz (Only valid, when the LPF is set CUSTom). |
|
Query Syntax |
ADEM:METR:FILT:LPF:CUT? |
|
Return Type |
<char> |
|
Default |
300 Hz |
Last Modified:
|
14june2021 |
New command (A.12.3x) |