|
(Read-Write) Set the channel equalization alignment to either FAST (default, when == 1). Or PRECISE when the channel equalization is set == 0. Note: This command applies only to B Series FieldFoxes with Option B04 /B10). |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<bool> |
Channel Scanner state. Choose from: 1 (ON) - The channel equalization alignment process occurs faster without the enhanced phase accuracy data (default). 0 (OFF) - The channel equalization alignment process time is longer due to additional channel equalization data being measured to enhance the phase accuracy. |
|
Examples |
ALIG:CHEQ:FAST 1 */Fast channel equalization alignment is accomplished with a single set of measurements (default). ALIG:CHEQ:FAST 0 */Precise channel equalization is accomplished using multiple sets of measurements for enhanced phase accuracy, but slower alignment time. |
|
Query Syntax |
[:SENSe]:ALIGnment:CHEQ:FAST? |
|
Return Type |
booleon |
|
Default |
1 (ON) |
Last Modified:
|
28oct2022 |
New command (A.12.5x) |