|
(Read-Write) Set and query the antenna's angle of azimuth (X) step value (1 to 10 degrees). |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<numeric> |
Set the antenna's angle azimuth step value: Set between: 1 to 10 degrees |
|
Examples |
ANT:ANG:AZIM:STEP 5 */Sets the angle azimuth step to 5 degrees |
|
Query Syntax |
ANT:ANG:AZIM:STEP? |
|
Return Type |
Numeric |
|
Default |
4 |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01dec019 |
New command |