|
(Read-Write) Set and query the antenna's angle of azimuth (X) stop value (-90 to 90 degrees). |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<numeric> |
Set the angle azimuth stop value: Set between: -89 and 90 degrees |
|
Examples |
ANT:ANG:AZIM:STOP -45 */Sets the angle azimuth stop to -45 degrees |
|
Query Syntax |
ANT:ANG:AZIM:STOP? |
|
Return Type |
Numeric |
|
Default |
90 |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01dec019 |
New command |