|
(Read-Write) Set and query the elevation angle (Y) reference value (-89 to 90 degrees). |
|
|
Relevant Modes |
|
|
Couplings |
Azimuth Reference and Elevation reference are dynamic based on any changes that occur to either value. |
|
Parameters |
|
|
<numeric> |
Set the angle elevation reference value: Set between: -89 and 90 degrees |
|
Examples |
ANT:ANG:AZIM:REF -45 */Sets the angle azimuth reference to -45 degrees |
|
Query Syntax |
ANT:ANG:AZIM:REF? |
|
Return Type |
Numeric |
|
Default |
0 |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01dec019 |
New command |