|
(Read-Write) Set and query the antenna's angle of elevation (Y) start value (-89 to 89 degrees). |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<numeric> |
Set the heat marker elevation value: Set between: -89 and 89 degrees |
|
Examples |
ANT:ANG:ELEV:STAR -45 */Sets the angle elevation start to -45 degrees |
|
Query Syntax |
ANT:ANG:ELEV:STAR? |
|
Return Type |
Numeric |
|
Default |
-89 |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01dec019 |
New command |