|
(Read-Write) Set and query the antenna's angle of azimuth (X) reference value. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<numeric> |
Set the angle azimuth index value: Set between: Set between Min: -1.00000000000000E+18 Max: 1.00000000000000E+32. |
|
Examples |
ANT:ANGL:IND:X -45 */Sets the angle azimuth index X to -4.50000000000000E+01 |
|
Query Syntax |
ANT:ANGL:IND:X? |
|
Return Type |
Double |
|
Default |
0.00000000000000E+18 |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01dec019 |
New command |