|
(Read-Write) Set and query the Polar display rotation. 0 degrees is vertical on display 90 degrees is horizontal on right side of display (-180 to 180 degrees). |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<numeric> |
Set the display polar angle value: Set between: -180 and 180 degrees |
|
Examples |
ANT:DISP:POL:ANGL 45 */Sets the polar angle value to 45 degrees |
|
Query Syntax |
ANT:DISP:POL:ANGL? |
|
Return Type |
Numeric |
|
Default |
0 |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01dec019 |
New command |