(Read-Write) Sets and queries the audio capture time (the length of the audio capture). . |
|
Relevant Modes |
|
Parameters |
|
<num> |
Capture time in seconds
Min: Dynamic. Varies based on the span/sample rate. Max: Dynamic. Varies based on the span/sample rate. |
Examples |
:AUD:CAPT:TIME .200 'Sets the audio capture time to 200 ms |
Query Syntax |
:AUD:CAPT:TIME? |
Return Type |
Numeric |
Default |
100 ms |
Last Modified:
14june2021 |
Added this command (A.12.3x) |