(Write-Read) Set and read the Cal Kit to use for the specified port number. |
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
Parameters |
|
<port> |
Port number for the Cal Kit. N9912A, choose 1 All other models, choose 1 or 2 |
<ckit> |
(String) Cal Kit for the specified port number. Case-sensitive. Use [:SENSe]:CORRection:COLLect:CKIT:LABel:CATalog? to read a list of valid Cal Kits. CORR:COLL:CKIT:LAB 1,"85052D" |
|
Using ECalECal modules that are connected to a FieldFox USB port with connectors that match the specified <port> are appended to the end of the list of valid Cal Kits that are returned using [:SENSe]:CORRection:COLLect:CKIT:LABel:CATalog?. NOTE: The ECal module MUST be connected. To specify an ECal module, instead of <ckit> use the following (String) syntax: <model>;[serial];[char index]
The following are valid ECal specifiers: 'Specify
all three arguments including User Char 1: 'The
first N4431A will be used with the Factory Characterization 'Use
the Factory Char. 'The
first N4431A will be used with User Char 1 |
Query Syntax |
[:SENSe]:CORRection:COLLect:CKIT:LABel? <port> |
Default |
Not Applicable |
Last Modified:
26-Jul-2013 |
Added ECal |
18-Oct-2012 |
Added new models |