|
(Write-Read) Set and read the DUT connector that will be connected to the specified FieldFox port. |
|
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
|
Parameters |
|
|
<port> |
Port number for the Cal Kit. N9912A, choose 1 All other models, choose 1 or 2 |
|
<type -gen-,imp> |
(String) Type, gender, and impedance of the DUT connector. > Type: choose from: Type N | 3.5 mm | 7 mm | 7/16 | Type F | WR-10 | WR-15 | WR-19 | WR-22 | WR-28 | WR-42 | WR-62 | WR-75 | WR-90 | WR-112 | WR-137 | WR-187 | WR-284 | WR-650 | Other
> Gender: choose from one of the following when the connector type includes gender. 7mm, 7/16, and waveguide (WR-nn) do NOT include gender.
> Impedance: choose from: 50 or 75.
A regular expression/compact sequence for the connector name could be expressed as: "[^\s].*( -M|F-)?,\d+"
|
|
Examples |
CORR:COLL:CONN 1,"Type N -M-,50" Correction:Collect:Connector 2, "7 mm,50" CORR:COLL:CONN 1, "WR-10,1" CORR:COLL:CONN 2, "WR-650,1" |
|
Query Syntax |
[:SENSe]:CORRection:COLLect:CONNector? <port> |
|
Default |
Not Applicable |
Last Modified:
|
22-Oct-2012 |
Updated for new models |
|
16-Feb-2011 |
Updated |