(Write-Read) Choose to receive a single prompt to connect the ECal or one for each reference plane. Note: This command should be sent before sending any of the SENS:CORR:COLL:METH commands. See Calibration Commands. |
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
Parameters |
|
<bool> |
Simple ECal state. Choose from the following: ON or 1 (default) - The FieldFox assumes that both ports of the ECal module can be connected at both calibration reference planes. You therefore receive a single prompt to connect the ECal module to both ports. OFF or 0- Select when physical restrictions prohibit the ECal module from being connected to both calibration reference planes simultaneously. You will receive separate prompts to connect the ECal module to Port 1, then to connect the ECal to Port 2. |
Examples |
CORR:COLL:ECAL:SIMP 1 Sense:Correction:Collect:Ecal:Simple off |
Query Syntax |
[:SENSe]:CORRection:COLLect:ECAL:SIMPle ? |
Default |
ON or 1 |
Last Modified:
1-Nov-2013 |
New command |