|
(Write-Only) Measures the standard for the specified step number in the guided cal. Use [:SENSe]:CORRection:COLLect:GUIDed:SCOunt to read the number of steps required for the cal. This command is overlapped. This means that it will execute and, while the FieldFox measures the cal standard, it will also accept new commands. Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands. |
|
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
|
Parameters |
|
|
<num> |
Step number of the guided calibration. |
|
Examples |
CORR:COLL:GUID:STEP:ACQ 1 |
|
Query Syntax |
Not Applicable |
|
Default |
Not Applicable |
Last Modified:
|
18-Oct-2012 |
New command |