[:SENSe]:CORRection:LOSS:BEFore[:VALue] <double>

(Read-Write) Set and query the amount of noise figure correction loss before the DUT input.

Use CORRection:LOSS:BEFore:ENABled to set the correction loss level before the DUT input.

Relevant Modes

NF

Parameters

 

<double>

Set the amount of noise figure loss correction before the DUT input. Choose from:

-100 to 100 dB - The correction loss value stated using the CORRection:LOSS:BEFore:ENABled  command.

0.00 dB - Default

Examples

:CORR:LOSS:BEF -15.55

Query Syntax

:CORRection:LOSS:BEFore?

Return Type

Double

Default

OFF


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)