|
(Write-Read) Set and query the calibration media type. If the measurement requires electrical delay or port extensions, available ONLY in NA Mode, you must specify the waveguide Media Type and Cutoff Frequency. These settings are needed to help specify dispersion. They are NOT used if electrical delay and port extensions are both zero. |
|
|
Relevant Modes |
NA, CAT |
|
Parameters |
|
|
<bool> |
Media type. Choose from the following: COAX - Calibration standards are coaxial. WAVeguide - Calibration standards are waveguide. |
|
Examples |
CORR:MED WAV Sense:Correction:Medium Waveguide |
|
Query Syntax |
[:SENSe]:CORRection:MEDium? |
|
Default |
COAX |
Last Modified:
|
1-Nov-2013 |
New command |