|
(Read-Write) Set and query the frequency of the power meter measurement. This is used to set the proper correction value of the power sensor. |
|
|
Relevant Modes |
Power Meter, Pulse Measurements, CPM |
|
Parameters |
|
|
<num> |
Frequency in Hz. Choose a number between the minimum and maximum frequency of the FieldFox. This command will accept MIN and MAX as arguments. |
|
Examples |
FREQ 10E6 FREQ MAX |
|
Query Syntax |
[:SENSe]:FREQuency? |
|
Return Type |
Numeric |
|
Default |
Center frequency of the FieldFox |
Last Modified:
|
1-Apr-2014 |
Added CPM |
|
29-Oct-2013 |
Added Pulse |