Built-in Power Meter (CPM) Mode Commands

See Also

- Commands that are Common to All Modes

- Status Registers


Frequency and Power

Description

Command

Set frequency

[:SENSe]:FREQuency

Step size for up/down keys

[:SENSe]:FREQuency:CENTer:STEP

Freq span

[:SENSe]:FREQuency:SPAN

Attenuation value

[:SENSe]:POWer[:RF]:ATTenuation

Radio Standard

Channel number center

[:SENSe]:RADio:CHANnel:CENTer

Uplink or Downlink

[:SENSe]:RADio:CHANnel:DIRection

Channel step size

[:SENSe]:RADio:CHANnel:STEP

Select standard

[:SENSe]:RADio:STANdard[:SELect]

Freq or Chan

[:SENSe]:RADio:TEUNit

Read Data

Read measurement data

[:SENSe]:TRACe[:DATA]?

Alignments (InstAlign)

Align all now (coupled to all individual alignments)

[:SENSe]:ALIGnment:ALL:NOW

Align all state (coupled to all individual alignments)

[:SENSe]:ALIGnment:ALL[:STATe]

Align now

[:SENSe]:ALIGnment:AMPLitude:NOW

InstAlign state

[:SENSe]:ALIGnment:AMPLitude[:STATe]

USB/LAN Power Sensor

Query the sensor's model number string and serial number string values

DISPlay:MODel:DATA

Enable/disable the model annotations

DISPlay:MODel:STATe

Set and query the LAN sensor's IP address

INPut:LAN:ADDRess

Set and query the LAN sensor's IP address

INPut:LAN:ID:NAME

Set and query the autogenerated hostname

INPut:LAN:ID:SNUMber

Set and query the hostname.

INPut:LAN:ID:TYPe

Set/query the USB or LAN power sensor type

INPut:TYPe

Display

Display units

[:SENSe]:AMPLitude:UNIT

Set Minimum scale value

DISPlay[:WINDow]:ANALog:LOWer

Set Maximum scale value

DISPlay[:WINDow]:ANALog:UPPer

Set PM resolution

DISPlay[:WINDow][:NUMeric]:RESolution

Enable averaging

[:SENSe]:AVERage[:ENABle]

Set number of sweep averages.

[:SENSe]:AVERage:COUNt

Make relative measurements

CALCulate:RELative[:MAGNitude]:AUTO

Set Offset value.

[:SENSe]:CORRection:GAIN2[:INPut][:MAGNitude]

Set Offset ON | OFF state

[:SENSe]:CORRection:GAIN2:STATe

Limit Lines

Set the minimum (lower) limit value.

[:SENSe]:TRACe:LIMit:LOWer

Set the lower ON | OFF State.

[:SENSe]:TRACe:LIMit:LOWer:STATe

Set the maximum (upper) limit value.

[:SENSe]:TRACe:LIMit:UPPer

Set the upper ON | OFF State.

[:SENSe]:TRACe:LIMit:UPPer:STATe


Last Modified:

1-Apr-2014

Added CPM commands (A.07.50)