[:SENSe]:FREQuency:CENTer <num>

(Read-Write) Set and query the center frequency of the trace. This is also used for single frequency (CW) traces, such as the frequency of power meter measurements.

Relevant Modes

CAT, EMI, IQA (Spectrum Only), NA, NF, SA, VVM, and RTSA

Parameters

 

<numeric>

Center frequency in Hz. Choose a number between the minimum and maximum frequency of the FieldFox.

This command will accept MIN and MAX as arguments.

Examples

FREQ:CENT 10E6

FREQ:CENT MAX

Query Syntax

[:SENSe]:FREQuency:CENTer?

Return Type

Numeric

Default

CAT, IQA, NA, NF, SA modes - Center frequency of the FieldFox.

VVM mode - 2 MHz


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)

22oct2017

Added IQA mode (10.1x)

10-june-2016

Added RTSA mode (9.50)