[:SENSe]:FREQuency:CENTer:STEP:AUTO <bool>

(Read-Write) Set and query the state of setting center frequency step size. Used with the front panel up/down keys.

Relevant Modes

EMI, SA, RTSA

Parameters

 

<bool>

Step size state. Choose from:

ON or 1 - Step size is set automatically. Each press of the ▲|▼ arrows increments or decrements the value by 1/10th (one division) of the current frequency span.

OFF or 0 - Step size is set manually with [:SENSe]:FREQuency:CENTer:STEP.

Examples

FREQ:CENT:STEP:AUTO 1

sense:frequency:center:step:auto off

Query Syntax

[:SENSe]:FREQuency:CENTer:STEP:AUTO?

Return Type

Boolean

Default

ON or 1


Last Modified:

10-june-2016

Added RTSA mode (9.50)