[:SENSe]:FREQuency:STARt <num>

(Read-Write) Set and query the start frequency of the trace.

Relevant Modes

CAT, EMI, NA, NF, SA, RTSA 

Parameters

 

<num>

Start frequency in Hz. Choose a number between the minimum and maximum frequency of the FieldFox.

This command will accept MIN and MAX as arguments.

Examples

FREQ:STAR 10E6

FREQ:STAR MIN

Query Syntax

[:SENSe]:FREQuency:STARt?

Return Type

Numeric

Default

Start frequency of the FieldFox


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)

10-june-2016

Added RTSA mode (9.50)