(Read-Write) Set and query the stop frequency of the trace. |
|
Relevant Modes |
CAT, EMI, NA, NF, RTSA, and SA |
Parameters |
|
<num> |
Stop frequency in Hz. Choose a number between the minimum and maximum frequency of the FieldFox. This command will accept MIN and MAX as arguments. |
Examples |
FREQ:STOP 10E6 FREQ:STOP MAX |
Query Syntax |
[:SENSe]:FREQuency: STOP? |
Return Type |
Numeric |
Default |
Stop frequency of the FieldFox |
Last Modified:
01-june-2018 |
Added Opt. 356 NF(10.3) |
10-june-2016 |
Added RTSA mode (9.50) |