This command has been replaced by [:SENSe]:ALIGnment:CHEQ:NOW. Learn about superseded commands.
(Write-only) A IF Flatness alignment is performed once just before the next sweep and applied to subsequent sweeps. If the FieldFox is not sweeping, a single sweep is triggered and alignment is performed. |
|
Relevant Modes |
IQA, RTSA |
Parameters |
None |
Examples |
IFFL:ALIG:NOW |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
Last Modified:
22nov2017 |
Updated as a superseded note & added IQA for backwards compatibility. |
20-sep-2016 |
Add new RTSA command(A.09.50) |