Replacement Commands


The following is a list of commands that have been replaced.

Superseded Commands

Superseded commands will continue to work in existing programs. However, the replacement command usually has more functionality and is recommended.

Superseded command

Replacement command

D.14.04 (D-series)

SYSTem:VVS:CURRent?

SYSTem:DCPS:CURRent?

SYSTem:VVS:ENABle

SYSTem:DCPS:ENABle

SYSTem:VVS:MAXCurrent?

SYSTem:DCPS:MAXCurrent?

SYSTem:VVS:MVOLtage?

SYSTem:DCPS:MVOLtage?

SYSTem:VVS:RVOLtage??

SYSTem:DCPS:RVOLtage?

SYSTem:VVS:VOLTage

SYSTem:DCPS:VOLTage

SYSTem:VVS:[STATe]?

SYSTem:DCPS[:STATe]?

A.13.00

SYSTem:ANTenna:USB:IMPort

SYSTem:ANTenna:EMF:IMPort

SYSTem:ANTenna:USB:AXIS

SYSTem:ANTenna:EMF:AXIS

SYSTem:ANTenna:USB:TYPe

SYSTem:ANTenna:EMF:TYPe

A.12.1x

CALCulate:MARKer:NOISe[:STATe]

CALCulate:MARKer:FUNCtion

RECPlayback:CONFig:FMTRigger:DATA

RECPlayback:CONFig:FMTRigger:LLData

CALCulate[:SELected]:LIMit:DATA

CALCulate:LIMit:LLData

CALCulate[:SELected]:LIMit:BEEP

CALCulate[:SELected]:LIMit:SOUNd

A.10.15

[:SENSe]:AMPLitude:ALIGnment:NOW (i.e., now reads: [:SENSe]:AMPLitude:ALIGnment[:OBSOLETE]:NOW)

[:SENSe]:ALIGnment:AMPLitude:NOW

[:SENSe]:AMPLitude:ALIGnment[:STATe]

(i.e., now reads: [:SENSe]:AMPLitude:ALIGnment[:OBSOLETE][:STATe])

[:SENSe]:ALIGnment:AMPLitude[:STATe]

 [:SENSe]:AMPLitude:CORRections[:STATe]

[:SENSe]:AMPLitude:CORRections:DISable

[:SENSe]:BURSt:AMPLitude:ALIGnment:NOW (i.e., now reads: [:SENSe]:BURSt:ALIGnment[:OBSOLETE][:NOW)

[:SENSe]:ALIGnment:BURSt:NOW

[:SENSe]:BURSt:AMPLitude:ALIGnment[:STATe] (i.e., now reads: [:SENSe]:BURSt:ALIGnment[:OBSOLETE][:STATe])

[:SENSe]:ALIGnment:BURSt[:STARt]

[:SENSe]:IFFLatness:AMPLitude:ALIGnment:NOW

[:SENSe]:ALIGnment:CHEQ:NOW

[:SENSe]:IFFLatness:AMPLitude:ALIGnment["STATe]

[:SENSe]:ALIGnment:CHEQ[:STATe]

SYSTem:PREFerences:SAADC

SYSTem:PREFerences:SA:EAOR

 

OBSOLETE commands

These commands will NOT continue to work in existing programs.

Obsolete command

Replacement command

[:SENSe]:TAListen:AVOLume (A.05.50)

SYSTem:AUDio:VOLume

[:SENSe]:RADio:STANdard (A.05.50)

[:SENSe]:RADio:STANdard[:SELect]

 


Last Modified:

06mar2024

Updated commands for (A.13.00)

01dec2020

Updated commands for (A.12.1x)

22nov2017

New alignment commands (A.10.15)

5-Aug-2011

New topic (A.05.50)