This command has been replaced by [:SENSe]:ALIGnment:CHEQ[:STATe]. Learn about superseded commands.
(Read-Write) Set and query the RTSA mode IF flatness amplitude alignment (InstAlign) state. |
|
Relevant Modes |
IQA, RTSA |
Parameters |
|
<char> |
InstAlign state. Choose from: AUTO - The alignment process is performed every 300 seconds or when the temperature has changed about 1 degree. It occurs only at the beginning of a sweep and takes about 0.5 seconds to complete. HOLD - The alignment process is stopped, but the last alignment values are applied to subsequent sweeps. OFF - The alignment process is NOT performed. Only factory correction values are used. |
Examples |
IFFL:ALIG HOLD |
Query Syntax |
[:SENSe]:IFFLatness:ALIGnment[:STATe]? |
Return Type |
Character |
Default |
AUTO |
Last Modified:
22nov2017 |
Updated as a superseded note & added IQA for backwards compatibility. |
20-sep-2016 |
Added RTSA command(A.09.50) |