[:SENSe]:IQSTream:ARP <bool>

(Read-Write) Set and query ARP (Address Resolution Protocol) refresh state.

Note: For enhanced mode streaming ONLY.

Note: This command applies to FieldFox D-series (Fluyt) models and above.

Relevant Modes

SA mode (IQ Streaming)

Parameters

 

<bool>

Set the ARP refresh state, choose from:

ON / 1 - Enable ARP refresh.

OFF / 0 - Disable ARP refresh.

Examples

IQST:ARP 1 'Enable the ARP refresh.

Query Syntax

IQST:ARP?

Return Type

bool

Default

ON

Last Modified:

25May2026

New command for D-series models (D.14.1x) and above.