[:SENSe]:IQSTream:ARP:DURAtion <int>

(Read-Write) Set and query ARP refresh rate in seconds.

Note: For enhanced mode streaming ONLY.

Note: This command applies to FieldFox D-series (Fluyt) models and above.

Relevant Modes

SA mode (IQ Streaming)

Parameters

 

<int>

Set the ARP refresh rate (seconds).

Examples

IQST:ARP:DURA 200 'Set the ARP refresh rate to 200 seconds.

Query Syntax

IQST:ARP:DURA?

Return Type

int

Default

128


Last Modified:

25May2026

New command for D-series models (D.14.1x) and above.