[:SENSe]:IQSTream:CONNection <enum>

(Read-Write) Set and query the IQ Streaming Connection Type.

Note: This command applies to FieldFox D-series (Fluyt) models and above.

Relevant Modes

SA mode (IQ Streaming)

Parameters

 

<enum>

IQ Streaming Connection Type choose from:

ETHernet - Set IQ streaming using 1G Ethernet connection.

TENGethernet - Set IQ streaming using 10G Ethernet connection.

FILesystem - Set IQ streaming recordiung.

Examples

IQST:CONN TENG 'Set the IQ Streaming Connection type to 10G Ethernet

Query Syntax

IQST:CONN?

Return Type

 enum

Default

ETH

Last Modified:

25May2026

New command D-series models (D.14.04) and above.