[:SENSe]:IQSTream:DIFI:IFRFrequency <float>

(Read-Write) Set and query the IF reference frequency used in DIFI contex packet.

Note: This command applies to FieldFox D-series (Fluyt) models and above.

Relevant Modes

SA mode (IQ Streaming)

Parameters

 

<float>

IF reference frequency.

Examples

IQST:DIFI:IFRF 12e6 'Set the IF referenec frequency 12 MHz used in DIFI contex packet.

Query Syntax

IQST:DIFI:IFRF?

Return Type

float

Default

0


Last Modified:

25May2026

New command for D-series models (D.14.1x) and above.