[:SENSe]:IQSTream:RFILename <string>

(Read-Write) Set and query the IQ Streaming Recording filename. This is the name of the recording folder that contains the .vita49 and SessionInfo.txt file for the recording. This name may contain a numeric suffix if another recording exists in the same folder. 

Note: This command applies to FieldFox D-series (Fluyt) models and above.

Relevant Modes

SA mode (IQ Streaming)

Parameters

 

<string>

IQ Streaming Recording Filename:

Examples

IQST:RFIL "" 'Set the IQ Streaming Recording Filename.

Query Syntax

IQST:RFIL?

Return Type

string

Default

"AutoIQRecording"


Last Modified:

25May2026

New command for D-series models (D.14.04) and above.